Genix Deployment Architecture - On Premise

The following figure depicts the architecture of on premise deployment in LAN network or Azure cloud data center as IaaS.

 Genix Deployment Architecture - On Premise

The on premise deployment comprises of the following two main sections:

  • Genix Edge Platform (Southbound)

  • Genix Analytics Platform (Northbound)

Genix Edge Platform Deployment

Genix Edge is deployed in edges. Edges are deployed in customer's LAN network (L3, L4) and connected to Genix northbound (L4).

Genix Genix Edge Platform Deployment is on a VM (Runtime environment - Ubuntu LTS, Docker, Docker Swarm).

Genix Analytics Platform

Genix Analytics Platform is deployed in L4 network using set of VMs. For information about the list of deployable components, see Infrastructure Requirements.